Part Number: C2000-GANG
Hi experts,
This is posted for information purposes only and is only one possible solution. Please note that this solution may not be valid.
[Usage environment]
- PC: Windows 10 Pro
- C2000-GANG(HW): 01.02
- C2000-GANG(firmware): 01.00.06
- C2000-GANG-SW(GUI): 01.00.06
- Device: TMD320F28075
[Error 27: Flash write err]
There are no reported cases of this error and the cause is unknown.
Error 27 occurred, when a modified C2000-GANG image file could not be written to a device that was being written to normally.
The situation is that the device can only be written to with an image file that was previously created.
→After updating the GANG software (firmware and GUI) to the latest version, it can now write without problems.(v01.01.10)
[Error 69: DSP firmware start]
This error has been reported in several cases, but this is a solution that has not been reported so far.
Error 69 occurred, when the same image file could not be written a second time to a device that was being written to normally.
→With the CLA running, the CPU cannot be accessed from GANG and ERR69 seems to occur (READ is also not possible).
If access from GANG is started immediately after the CPU is switched on (before the CLA starts operating), it can now be written without problems.
Also, if the CLA process in the programme is commented out, it can now write without problems.
Best regards,
O.H