Part Number: TMS320F28027
Other Parts Discussed in Thread: C2000WARE
I have a new project copied from an existing project. The new project does not run from Flash without the debugger connected. One difference that I am focused on right now is that the old project has a "codestart" symbol shown in the map file. The new project is missing codestart.
How do I properly configure project settings, etc., so that it starts up from Flash without the debugger connected?
Some background on what I have looked at so far:
For the new project, I am using c2000ware\device_support\f2802x\common\ccs\Debug\driverlib.lib
Using nm2000 to show the symbol table, this copy of driverlib.lib has a codestart symbol. As I said, it is not showing up in the map file for the project.
The project configuration between old and new projects is the same. It is possible that I am missing some setting.
(I do not have all of the build files for the old project so I am not able to build it. I am told it is working standalone)
From the sample project Example_F2802xLEDBlink, I see a setting for specifying entry point, where that sample project has this set to code_start. I made the same setting in my project, then I get an error:
Description Resource Path Location Type
unresolved symbol _c_int00, first referenced in C:/ti/c2000/C2000Ware_MotorControl_SDK_4_02_00_00/c2000ware/device_support/f2802x/common/ccs/Debug/driverlib.lib<f2802xx_codestartbranch.obj> TitanCube_Ctrl_PC C/C++ Problem
I saw that Example_F2802xLEDBlink includes "rts2800_ml.lib" under the Linker "File Search Path"
I added "rts2800_ml.lib". Then I get a warning:
Description Resource Path Location Type
entry-point symbol other than "_c_int00" specified: "code_start" TitanCube_Ctrl_PC C/C++ Problem
The new project runs with the debugger, and now without the debugger.
If I remove the "code_start" now, the warning goes away, but the project no longer runs from Flash.
So adding code_start back into the linker settings, it seems I have a solution, but why do I get the warning? What is the "right way" to do this?
Thanks!