Part Number: TIEVM-HV-1PH-DCAC
Hi Team,
A customer of mine requested our TIEVM-HV-1PH-DCAC board. From receiving the board, the board cannot power up on their workbench. Can you please help answer their concerns below:
1. For software issue, How to setup for this?
Do you have any good solutions for the problem of DEBUG errors?


2. According to the setting in chapter 3.1.2.3.1.5, EPwm1Regs.TZFLG. cannot be set to zero, The boardStatus not set to boardStatus_NoFault.boardStatus is always in the state of boardSTatus_OverCurrentTrip, and there is no input voltage at this time. When the input voltage is 50V, there is no output waveform. When the input voltage rises to 380V, guiVbus does not update 380V, and there is no output voltage. Can you help me with this question?

Thanks!
BR,
Alfred