Part Number: TMS320F28335
HI TEAMS:
The main chip TMS320F28335PTPQ currently in use has encountered an abnormal current sampling problem during the client's use. After investigation, it has been confirmed that the main problem is the chip experiencing abnormalities in a high-temperature environment. The main phenomenon is:
1. The single board operates in a high-temperature environment, and there is a jump in the current sampling value. After investigation, it is found that the input signal of the current sampling pins (ADCINA0, ADCINA1, ADCINA2) of the main chip is normal, but there is a jump in the register value;
2. Under the ambient temperature of+75 ℃~+85 ℃, abnormal jumps will occur in the sampling values. The higher the temperature, the more frequent the sampling value jumps.
3. There are currently 4 PCS with this issue
Could you please help me point out where the problem lies or how to solve it?