This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LAUNCHXL-F28379D: Issue with DAC

Part Number: LAUNCHXL-F28379D


Hello E2E community,

I need to monitor some signals from a Simulink file in external mode on an oscilloscope using the DAC block from the Launchpad F28379 library. I attempted to connect it; however, when I begin generating code with the DAC connected, the external mode is terminated.

I was wondering if any one could help out with this.

I have attached a screenshot of the component

Regards,

Mohamed