This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: program error

Part Number: TMS320F28027
Other Parts Discussed in Thread: CONTROLSUITE

dear  

       For now, I've configured the application according to the Building Static Library appendix in the EC60730 Reference Manual. I also downloaded the controlsuit from the TI website to meet the requirements for the include options configuration, as shown below

 program show:  pTimerRegister->TCR.bit.TSS = 1U;  // stop time

error:Description Resource Path Location Type
#395 pointer to incomplete class type is not allowed STL_timer_test.c /IEC60730_f28027 line 106 C/C++ Problem

any advice?thanks in advance

  • Hello Raymond,

    Is this project based on an example from ControlSUITE or is this your own program using ControlSUITE? Also, if you check Resources -> Linked Resources are the file paths pointing to the proper locations for each variable name?

    Best regards,

    Omer Amir