This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280025: Boot Configuration through SCI

Part Number: TMS320F280025

Hi,

Good Day.

The customer is using the TMS320F280025 controller.

They are facing issues, in booting. Initially, the booting is working properly but it couldn't able to come out from boot mode after completing of the booting process.

We have set, the default boot modes as given: GPIO24 is 0 and GPIO32 is 1 for booting.

Please suggest which pins need to be high and low to come out of booting mode (out from programming).

Best Regards,

Ray Vincent