Other Parts Discussed in Thread: C2000WARE
Hello All,
I am using the code, epwm_ex13_up_aq.c .I have attached the code here.
The objective is:
1) To vary the duty cycle upto 50% and fix it at 50%.
2) give a phase shift defined by the variable "Ph" in watchdog
To achieve this, I have two flags: AshikFlag and loop_counter in watchdog. To enable the phase shift, the loop_counter should be equal to AshikFlag.
There are some challenges I am facing:
1) At higher frequencies, when I change the loop_counter to AshikFlag, EPWM2 becomes unstable. I think its' because I put a hardcode in isr function of EPWM2. Is there any smarter way to do it?
The code is added.
Thanks.
Ashik
//###########################################################################
//
// FILE: epwm_ex13_up_aq.c
//
// TITLE: Action Qualifier Module - Using up count.
//
//! \addtogroup driver_example_list
//! <h1> EPWM Action Qualifier (epwm_up_aq)</h1>
//!
//! This example configures ePWM1, ePWM2, ePWM3 to produce an
//! waveform with independent modulation on EPWMxA and
//! EPWMxB.
//!
//! The compare values CMPA and CMPB are modified within the ePWM's ISR.
//!
//! The TB counter is in up count mode for this example.
//!
//! View the EPWM1A/B(GPIO0 & GPIO1), EPWM2A/B(GPIO2 & GPIO3)
//! and EPWM3A/B(GPIO4 & GPIO5) waveforms via an oscilloscope.
//!
//
//###########################################################################
//
//
// $Copyright:
// Copyright (C) 2021 Texas Instruments Incorporated - http://www.ti.com/
//
// Redistribution and use in source and binary forms, with or without
// modification, are permitted provided that the following conditions
// are met:
//
// Redistributions of source code must retain the above copyright
// notice, this list of conditions and the following disclaimer.
//
// Redistributions in binary form must reproduce the above copyright
// notice, this list of conditions and the following disclaimer in the
// documentation and/or other materials provided with the
// distribution.
//
// Neither the name of Texas Instruments Incorporated nor the names of
// its contributors may be used to endorse or promote products derived
// from this software without specific prior written permission.
//
// THIS SOFTWARE IS PROVIDED BY THE COPYRIGHT HOLDERS AND CONTRIBUTORS
// "AS IS" AND ANY EXPRESS OR IMPLIED WARRANTIES, INCLUDING, BUT NOT
// LIMITED TO, THE IMPLIED WARRANTIES OF MERCHANTABILITY AND FITNESS FOR
// A PARTICULAR PURPOSE ARE DISCLAIMED. IN NO EVENT SHALL THE COPYRIGHT
// OWNER OR CONTRIBUTORS BE LIABLE FOR ANY DIRECT, INDIRECT, INCIDENTAL,
// SPECIAL, EXEMPLARY, OR CONSEQUENTIAL DAMAGES (INCLUDING, BUT NOT
// LIMITED TO, PROCUREMENT OF SUBSTITUTE GOODS OR SERVICES; LOSS OF USE,
// DATA, OR PROFITS; OR BUSINESS INTERRUPTION) HOWEVER CAUSED AND ON ANY
// THEORY OF LIABILITY, WHETHER IN CONTRACT, STRICT LIABILITY, OR TORT
// (INCLUDING NEGLIGENCE OR OTHERWISE) ARISING IN ANY WAY OUT OF THE USE
// OF THIS SOFTWARE, EVEN IF ADVISED OF THE POSSIBILITY OF SUCH DAMAGE.
// $
//###########################################################################
//
// Included Files
//
#include "driverlib.h"
#include "device.h"
#include "board.h"
//
// Defines
//
#define EPWM1_TIMER_TBPRD 100 // Period register //2000
#define EPWM1_MAX_CMPA 50 //1000
#define EPWM1_MIN_CMPA 0
#define EPWM1_MAX_CMPB 50 //1000
#define EPWM1_MIN_CMPB 0
#define EPWM2_TIMER_TBPRD 100 // Period register
#define EPWM2_MAX_CMPA 50 //1950
#define EPWM2_MIN_CMPA 0 //50
#define EPWM2_MAX_CMPB 50 //1950
#define EPWM2_MIN_CMPB 0 //50
#define EPWM3_TIMER_TBPRD 100 // Period register
#define EPWM3_MAX_CMPA 50
#define EPWM3_MIN_CMPA 0
#define EPWM3_MAX_CMPB 50
#define EPWM3_MIN_CMPB 0
#define EPWM_CMP_UP 1
#define EPWM_CMP_DOWN 0
//
// Globals
//
typedef struct
{
uint32_t epwmModule;
uint16_t epwmCompADirection;
uint16_t epwmCompBDirection;
uint16_t epwmTimerIntCount;
uint16_t ePWMDone;
uint16_t epwmMaxCompA;
uint16_t epwmMinCompA;
uint16_t epwmMaxCompB;
uint16_t epwmMinCompB;
} epwmInfo;
epwmInfo epwm1Info;
epwmInfo epwm2Info;
epwmInfo epwm3Info;
uint16_t AshikFlag = 0 ; //Ashik Added
uint16_t Ph = 0 ; //Ashik Added
uint16_t loop_counter = 0 ; //Ashik Added
volatile uint16_t compAVal, compBVal;
//
// Function Prototypes
//
void initEPWM1(void);
void initEPWM2(void);
void initEPWM3(void);
__interrupt void epwm1ISR(void);
__interrupt void epwm2ISR(void);
__interrupt void epwm3ISR(void);
void updateCompare(epwmInfo*);
//
// Main
//
void main(void)
{
//
// Initialize device clock and peripherals
//
Device_init();
//
// Disable pin locks and enable internal pull-ups.
//
Device_initGPIO();
//
// Initialize PIE and clear PIE registers. Disables CPU interrupts.
//
Interrupt_initModule();
//
// Initialize the PIE vector table with pointers to the shell Interrupt
// Service Routines (ISR).
//
Interrupt_initVectorTable();
//
// For this case just init GPIO pins for ePWM1, ePWM2, ePWM3
//
Board_init();
//
// Interrupts that are used in this example are re-mapped to
// ISR functions found within this file.
//
Interrupt_register(INT_EPWM1, &epwm1ISR);
Interrupt_register(INT_EPWM2, &epwm2ISR);
Interrupt_register(INT_EPWM3, &epwm3ISR);
//
// Disable sync(Freeze clock to PWM as well)
//
SysCtl_disablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
// Initialize PWM1 without phase shift as master
initEPWM1();
// Initialize PWM2 with phase shift of X
initEPWM2();
//EPWM_selectPeriodLoadEvent(myEPWM2_BASE, EPWM_SHADOW_LOAD_MODE_SYNC);
//EPWM_setPhaseShift(myEPWM2_BASE, Ph); //ashik added Ph
// EPWM_setTimeBaseCounter(myEPWM2_BASE, Ph); //ashik added Ph
initEPWM3();
EPWM_setSyncOutPulseMode(EPWM1_BASE, EPWM_SYNC_OUT_PULSE_ON_COUNTER_ZERO);
//
// ePWM2 uses the ePWM 1 SYNCO as its SYNCIN.
// ePWM2 SYNCO is generated from its SYNCIN, which is ePWM1 SYNCO
//
EPWM_setSyncOutPulseMode(myEPWM2_BASE, EPWM_SYNC_OUT_PULSE_ON_EPWMxSYNCIN);
//
// ePWM4 uses the ePWM 1 SYNCO as its SYNCIN.
//
//SysCtl_setSyncInputConfig(SYSCTL_SYNC_IN_EPWM4, SYSCTL_SYNC_IN_SRC_EPWM1SYNCOUT);
//
// Enable all phase shifts.
//
EPWM_enablePhaseShiftLoad(myEPWM2_BASE);
//
// Enable sync and clock to PWM
//
SysCtl_enablePeripheral(SYSCTL_PERIPH_CLK_TBCLKSYNC);
//
// Enable interrupts required for this example
//
Interrupt_enable(INT_EPWM1);
Interrupt_enable(INT_EPWM2);
Interrupt_enable(INT_EPWM3);
//
// Enable global Interrupts and higher priority real-time debug events:
//
EINT; // Enable Global interrupt INTM
ERTM; // Enable Global realtime interrupt DBGM
//
// IDLE loop. Just sit and loop forever (optional):
//
for(;;)
{
asm (" NOP");
}
}
//
// epwm1ISR - EPWM1 ISR to update compare values
//
__interrupt void epwm1ISR(void)
{
//
// Update the CMPA and CMPB values
//
updateCompare(&epwm1Info);
//
// Clear INT flag for this timer
//
EPWM_clearEventTriggerInterruptFlag(myEPWM1_BASE);
//
// Acknowledge this interrupt to receive more interrupts from group 3
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}
//
// epwm2ISR - EPWM2 ISR to update compare values
//
__interrupt void epwm2ISR(void)
{
//
// Update the CMPA and CMPB values
//
if (loop_counter!=AshikFlag)
{
updateCompare(&epwm2Info);
}
else
{
//Ph=300;
EPWM_selectPeriodLoadEvent(myEPWM2_BASE, EPWM_SHADOW_LOAD_MODE_SYNC);
EPWM_setPhaseShift(myEPWM2_BASE, Ph); //ashik added Ph
EPWM_setTimeBaseCounter(myEPWM2_BASE, Ph); //ashik added Ph
}
//
// Clear INT flag for this timer
//
EPWM_clearEventTriggerInterruptFlag(myEPWM2_BASE);
//
// Acknowledge this interrupt to receive more interrupts from group 3
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}
//
// epwm3ISR - EPWM3 ISR to update compare values
//
__interrupt void epwm3ISR(void)
{
//
// Update the CMPA and CMPB values
//
updateCompare(&epwm3Info);
//
// Clear INT flag for this timer
//
EPWM_clearEventTriggerInterruptFlag(myEPWM3_BASE);
//
// Acknowledge this interrupt to receive more interrupts from group 3
//
Interrupt_clearACKGroup(INTERRUPT_ACK_GROUP3);
}
//
// initEPWM1 - Initialize EPWM1 values
//
void initEPWM1()
{
//
// Setup TBCLK
//
EPWM_setTimeBaseCounterMode(myEPWM1_BASE, EPWM_COUNTER_MODE_UP);
EPWM_setTimeBasePeriod(myEPWM1_BASE, EPWM1_TIMER_TBPRD);
EPWM_disablePhaseShiftLoad(myEPWM1_BASE);
EPWM_setPhaseShift(myEPWM1_BASE, 0U);
EPWM_setTimeBaseCounter(myEPWM1_BASE, 0U);
//
// Set ePWM clock pre-scaler
//
EPWM_setClockPrescaler(myEPWM1_BASE,
EPWM_CLOCK_DIVIDER_2,
EPWM_HSCLOCK_DIVIDER_2);
//
// Setup shadow register load on ZERO
//
EPWM_setCounterCompareShadowLoadMode(myEPWM1_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
EPWM_setCounterCompareShadowLoadMode(myEPWM1_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
//
// Set Compare values
//
EPWM_setCounterCompareValue(myEPWM1_BASE, EPWM_COUNTER_COMPARE_A,
EPWM1_MIN_CMPA);
EPWM_setCounterCompareValue(myEPWM1_BASE, EPWM_COUNTER_COMPARE_B,
EPWM1_MIN_CMPB);
//
// Set actions for ePWM1A & ePWM1B
//
// Set PWM1A on Zero
EPWM_setActionQualifierAction(myEPWM1_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
// Clear PWM1A on event A, up count
EPWM_setActionQualifierAction(myEPWM1_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
// Set PWM1B on Zero
EPWM_setActionQualifierAction(myEPWM1_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
// Clear PWM1B on event B, up count
EPWM_setActionQualifierAction(myEPWM1_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
// // Set PWM1B on Zero
// EPWM_setActionQualifierAction(myEPWM1_BASE,
// EPWM_AQ_OUTPUT_B,
// EPWM_AQ_OUTPUT_HIGH,
// EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
// // Clear PWM1B on event B, up count
// EPWM_setActionQualifierAction(myEPWM1_BASE,
// EPWM_AQ_OUTPUT_B,
// EPWM_AQ_OUTPUT_LOW,
// EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
//
// Interrupt where we will change the Compare Values
//
EPWM_setInterruptSource(myEPWM1_BASE, EPWM_INT_TBCTR_ZERO);
EPWM_enableInterrupt(myEPWM1_BASE);
EPWM_setInterruptEventCount(myEPWM1_BASE, 3U);
//
// Information this example uses to keep track
// of the direction the CMPA/CMPB values are
// moving, the min and max allowed values and
// a pointer to the correct ePWM registers
//
// Start by increasing CMPA & CMPB
epwm1Info.epwmCompADirection = EPWM_CMP_UP;
epwm1Info.epwmCompBDirection = EPWM_CMP_UP;
// Clear interrupt counter
epwm1Info.epwmTimerIntCount = 0;
epwm1Info.ePWMDone = 0;
// Set base as ePWM1
epwm1Info.epwmModule = myEPWM1_BASE;
// Setup min/max CMPA/CMP values
epwm1Info.epwmMaxCompA = EPWM1_MAX_CMPA;
epwm1Info.epwmMinCompA = EPWM1_MIN_CMPA;
epwm1Info.epwmMaxCompB = EPWM1_MAX_CMPB;
epwm1Info.epwmMinCompB = EPWM1_MIN_CMPB;
}
//
// initEPWM2 - Initialize EPWM2 values
//
void initEPWM2()
{
//
// Setup TBCLK
//
EPWM_setTimeBaseCounterMode(myEPWM2_BASE, EPWM_COUNTER_MODE_UP);
EPWM_setTimeBasePeriod(myEPWM2_BASE, EPWM2_TIMER_TBPRD);
EPWM_disablePhaseShiftLoad(myEPWM2_BASE);
EPWM_setPhaseShift(myEPWM2_BASE, 0U);
EPWM_setTimeBaseCounter(myEPWM2_BASE, 0U);
//
// Set ePWM clock pre-scaler
//
EPWM_setClockPrescaler(myEPWM2_BASE,
EPWM_CLOCK_DIVIDER_2,
EPWM_HSCLOCK_DIVIDER_2);
//
// Setup shadow register load on ZERO
//
EPWM_setCounterCompareShadowLoadMode(myEPWM2_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
EPWM_setCounterCompareShadowLoadMode(myEPWM2_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
//
// Set Compare values
//
EPWM_setCounterCompareValue(myEPWM2_BASE, EPWM_COUNTER_COMPARE_A,
EPWM2_MIN_CMPA);
EPWM_setCounterCompareValue(myEPWM2_BASE, EPWM_COUNTER_COMPARE_B,
EPWM2_MIN_CMPB); //EPWM2_MAX_CMPB
//
// Set actions for ePWM1A & ePWM1B
//
// Clear PWM2A on period and set on event A, up-count
// EPWM_setActionQualifierAction(myEPWM2_BASE,
// EPWM_AQ_OUTPUT_A,
// EPWM_AQ_OUTPUT_LOW,
// EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD);
// EPWM_setActionQualifierAction(myEPWM2_BASE,
// EPWM_AQ_OUTPUT_A,
// EPWM_AQ_OUTPUT_HIGH,
// EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
// Clear PWM2A on period and set on event A, up-count
EPWM_setActionQualifierAction(myEPWM2_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);// EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD
EPWM_setActionQualifierAction(myEPWM2_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
// Clear PWM2B on Period & set on event B, up-count
EPWM_setActionQualifierAction(myEPWM2_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);// EPWM_AQ_OUTPUT_ON_TIMEBASE_PERIOD
EPWM_setActionQualifierAction(myEPWM2_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
//
// Interrupt where we will change the Compare Values
//
EPWM_setInterruptSource(myEPWM2_BASE, EPWM_INT_TBCTR_ZERO);
EPWM_enableInterrupt(myEPWM2_BASE);
EPWM_setInterruptEventCount(myEPWM2_BASE, 3U);
//
// Information this example uses to keep track
// of the direction the CMPA/CMPB values are
// moving, the min and max allowed values and
// a pointer to the correct ePWM registers
//
// Start by increasing CMPA & decreasing CMPB
epwm2Info.epwmCompADirection = EPWM_CMP_UP;
epwm2Info.epwmCompBDirection = EPWM_CMP_DOWN;
// Clear interrupt counter
epwm2Info.epwmTimerIntCount = 0;
// Set base as ePWM2
epwm2Info.epwmModule = myEPWM2_BASE;
// Setup min/max CMPA/CMP values
epwm2Info.epwmMaxCompA = EPWM2_MAX_CMPA;
epwm2Info.epwmMinCompA = EPWM2_MIN_CMPA;
epwm2Info.epwmMaxCompB = EPWM2_MAX_CMPB;
epwm2Info.epwmMinCompB = EPWM2_MIN_CMPB;
}
//
// initEPWM3 - Initialize EPWM3 values
//
void initEPWM3(void)
{
//
// Setup TBCLK
//
EPWM_setTimeBaseCounterMode(myEPWM3_BASE, EPWM_COUNTER_MODE_UP);
EPWM_setTimeBasePeriod(myEPWM3_BASE, EPWM3_TIMER_TBPRD);
EPWM_disablePhaseShiftLoad(myEPWM3_BASE);
EPWM_setPhaseShift(myEPWM3_BASE, 0U);
EPWM_setTimeBaseCounter(myEPWM3_BASE, 0U);
//
// Set ePWM clock pre-scaler
//
EPWM_setClockPrescaler(myEPWM3_BASE,
EPWM_CLOCK_DIVIDER_1,
EPWM_HSCLOCK_DIVIDER_1);
//
// Setup shadow register load on ZERO
//
EPWM_setCounterCompareShadowLoadMode(myEPWM3_BASE,
EPWM_COUNTER_COMPARE_A,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
EPWM_setCounterCompareShadowLoadMode(myEPWM3_BASE,
EPWM_COUNTER_COMPARE_B,
EPWM_COMP_LOAD_ON_CNTR_ZERO);
//
// Set Compare values
//
EPWM_setCounterCompareValue(myEPWM3_BASE, EPWM_COUNTER_COMPARE_A,
EPWM3_MIN_CMPA);
EPWM_setCounterCompareValue(myEPWM3_BASE, EPWM_COUNTER_COMPARE_B,
EPWM3_MAX_CMPB);
//
// Set actions for ePWM1A & ePWM1B
//
// Set PWM3A on event B, up-count & clear on event B, up-count
EPWM_setActionQualifierAction(myEPWM3_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_HIGH,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPA);
EPWM_setActionQualifierAction(myEPWM3_BASE,
EPWM_AQ_OUTPUT_A,
EPWM_AQ_OUTPUT_LOW,
EPWM_AQ_OUTPUT_ON_TIMEBASE_UP_CMPB);
// Toggle EPWM3B on counter = zero
EPWM_setActionQualifierAction(myEPWM3_BASE,
EPWM_AQ_OUTPUT_B,
EPWM_AQ_OUTPUT_TOGGLE,
EPWM_AQ_OUTPUT_ON_TIMEBASE_ZERO);
//
// Interrupt where we will change the Compare Values
//
EPWM_setInterruptSource(myEPWM3_BASE, EPWM_INT_TBCTR_ZERO);
EPWM_enableInterrupt(myEPWM3_BASE);
EPWM_setInterruptEventCount(myEPWM3_BASE, 3U);
//
// Information this example uses to keep track
// of the direction the CMPA/CMPB values are
// moving, the min and max allowed values and
// a pointer to the correct ePWM registers
//
// Start by increasing CMPA & decreasing CMPB
epwm3Info.epwmCompADirection = EPWM_CMP_UP;
epwm3Info.epwmCompBDirection = EPWM_CMP_UP;
// Start the count at 0
epwm3Info.epwmTimerIntCount = 0;
// Set base as ePWM1
epwm3Info.epwmModule = myEPWM3_BASE;
// Setup min/max CMPA/CMP values
epwm3Info.epwmMaxCompA = EPWM3_MAX_CMPA;
epwm3Info.epwmMinCompA = EPWM3_MIN_CMPA;
epwm3Info.epwmMaxCompB = EPWM3_MAX_CMPB;
epwm3Info.epwmMinCompB = EPWM3_MIN_CMPB;
}
//
// updateCompare - Update the compare values for the specified EPWM
//
void updateCompare(epwmInfo *epwm_info)
{
//
// Every 10'th interrupt, change the CMPA/CMPB values
//
if(epwm_info->epwmTimerIntCount == 10)
{
epwm_info->epwmTimerIntCount = 0;
compAVal = EPWM_getCounterCompareValue(epwm_info->epwmModule,
EPWM_COUNTER_COMPARE_A);
compBVal = EPWM_getCounterCompareValue(epwm_info->epwmModule,
EPWM_COUNTER_COMPARE_B);
// if (compAVal==epwm_info->epwmMaxCompA) {epwm1Info.ePWMDone = 1;}
//
// If we were increasing CMPA, check to see if
// we reached the max value. If not, increase CMPA
// else, change directions and decrease CMPA
//
if(epwm_info->epwmCompADirection == EPWM_CMP_UP)
{
if(compAVal < epwm_info->epwmMaxCompA)
{
EPWM_setCounterCompareValue(epwm_info->epwmModule,
EPWM_COUNTER_COMPARE_A, ++compAVal);
AshikFlag = AshikFlag+1;
}
else
{
// epwm_info->epwmCompADirection = EPWM_CMP_DOWN;
// EPWM_setCounterCompareValue(epwm_info->epwmModule,
// EPWM_COUNTER_COMPARE_A, --compAVal);
// epwm1Info.ePWMDone = 1;
}
}
//
// If we were decreasing CMPA, check to see if
// we reached the min value. If not, decrease CMPA
// else, change directions and increase CMPA
//
else
{
if(compAVal == epwm_info->epwmMinCompA)
{
epwm_info->epwmCompADirection = EPWM_CMP_UP;
EPWM_setCounterCompareValue(epwm_info->epwmModule,
EPWM_COUNTER_COMPARE_A, ++compAVal);
}
else
{
EPWM_setCounterCompareValue(epwm_info->epwmModule,
EPWM_COUNTER_COMPARE_A, --compAVal);
}
}
//
// If we were increasing CMPB, check to see if
// we reached the max value. If not, increase CMPB
// else, change directions and decrease CMPB
//
if(epwm_info->epwmCompBDirection == EPWM_CMP_UP)
{
if(compBVal < epwm_info->epwmMaxCompB)
{
EPWM_setCounterCompareValue(epwm_info->epwmModule,
EPWM_COUNTER_COMPARE_B, ++compBVal);
}
else
{
// epwm_info->epwmCompBDirection = EPWM_CMP_DOWN;
// EPWM_setCounterCompareValue(epwm_info->epwmModule,
// EPWM_COUNTER_COMPARE_B, --compBVal);
}
}
//
// If we were decreasing CMPB, check to see if
// we reached the min value. If not, decrease CMPB
// else, change directions and increase CMPB
//
else
{
if(compBVal == epwm_info->epwmMinCompB)
{
epwm_info->epwmCompBDirection = EPWM_CMP_UP;
EPWM_setCounterCompareValue(epwm_info->epwmModule,
EPWM_COUNTER_COMPARE_B, ++compBVal);
}
else
{
EPWM_setCounterCompareValue(epwm_info->epwmModule,
EPWM_COUNTER_COMPARE_B, --compBVal);
}
}
}
//
// Increment interrupt count if < 10
//
else
{
epwm_info->epwmTimerIntCount++;
}
return;
}
//
// End of file
//