Part Number: TMS320F280039C
Hi team,
As shown in the figure below, the DSP supply voltage is 3.3 V. This chip has two pins, 78 and 79, as output pins, which theoretically output PWM complementary signals. Due to solder failure, two pins have been shorted. This is where the 78,79 output signal high level is around 1.6V.

As shown in the figure below, the yellow color shows the 78 and 79 port output waveform after the short. Why is the 78,79 GPIO port high only about 1.6V?


Could you help check this case? Thanks.
Best Regards,
Cherry