This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BLDC motor control

I have to control a BLDC motor powered between +9/32VDC @ 50A and peak current of 75A.

It is a direction and speed control type.

I am a little lost in the choice of microcontroller allowing such an application. Could I be contacted by an application engineer so that he can advise me on a standard hardware structure for this type of application and mainly about the microcontroller choice.