Hi experts,
Can XDS110 debugger or any other debugger read Flashpro2000's checksum code directly? Or is there any other better ways to read it? Thanks!
BR
Jim
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi experts,
Can XDS110 debugger or any other debugger read Flashpro2000's checksum code directly? Or is there any other better ways to read it? Thanks!
BR
Jim
Hi Jim,
I don't understand what you are asking. Can you clarify?
Hi Gus,
Sorry for my unclear description. This case is that the customer uses flashpro2000 to burn the firmware into the flash, can we connect the MCU through the emulator (XDS110) to read the checksum of the firmware? Or which emulator can read the checksum of the firmware burned?
Thanks!
BR
Jim
Jim,
The XDS110 has access to the MCU's flash, RAM and peripheral registers. If the checksum is stored in flash, and there is no MCU security feature enabled, the XDS110 should be capable of accessing the information.