Is there a mechanism to ensure the ADCSOCFLG1 or ADCSOCOVF1 register is 0 after one conversion?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Is there a mechanism to ensure the ADCSOCFLG1 or ADCSOCOVF1 register is 0 after one conversion?
Hi,
The ADCSOCFLG1 bit for a given SOC will be set to 0 when a conversion starts for that SOC. If another conversion is triggered while the previous conversion is still ongoing, then the ADCSOCFLG1 will be set to one until the next conversion starts.

Best Regards,
Ben Collier
Is there a mechanism to ensure soc won't miss any bit of 1 flag after one conversion?
To make sure AD conversion occurs on each expected channel, the software may be added a line of check statements like " if (ADCSOCFLG1==0)". If the chip itself has a similar confirmation mechanism to check it? If it doesn't have one, where can this line be added to ensure that the stability of the entire code project is not affected?
Hi Anka,
Are you trying to make sure that the ADC will not miss a conversion if the ADCSOCFLG1 already is set to 1? What is being used as the trigger for the ADC?
Best Regards,
Ben Collier