Part Number: TMS320F2812
Greetings,
I am building a library using compiler TI v20.2.5.LTS. When the link with the main project occurs, it is unable to find some of the functions in the library. Looking at one of them, it is in an assembly file which I can see was built because these is an object file for it. But ar2000 shows that the library does not contain it, and the map file contains the following:
n/a UNDEFED _<missing_routine>
It is being used by routines which are outside of the library. Is there an option which will force it to be included in the library?
Thank you,
Ed