Part Number: TMS320F28379D
Other Parts Discussed in Thread: UNIFLASH
I have problem load program into Microcontroller. The device I am using are TMS320F28379D, and the JTAG I am using are XDS110 USB Debug probe.
When I am trying to load the program using CCS or Uniflash, I keep getting error message like this:
[ERROR] C28xx_CPU1: Trouble Reading Register PC: (Error -1156 @ 0x0) Device may be operating in low-power mode. Do you want to bring it out of this mode? Choose 'Yes' to force the device to wake up and retry the operation. Choose 'No' to retry the operation without waking the device. (Emulation package 9.11.0.00128)
It will do nothing wether I select Yes or no to wake up the device.
Do you know why and how can I solve the issue?