This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28027: Max EPWM frequency

Part Number: TMS320F28027

Can you confirm the max operating frequency of the EPWM?

I have the CPU / SYSCLK configured for 60MHz.

Looking at the datasheet, I think max frequency of the EPWM is 33MHz.

But I have a project from another user that I think is based on TI sample code, where the ePWM is configured with HSPCLKDIV and CLKDIV both set to /1, or 60MHz.   The project seems to work okay.  So I just want to confirm.

Thanks!