This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28062: compiler version

Part Number: TMS320F28062

Depending on the version of the compiler, the compiled HEX file and MAP file are different for the same project. How can we ensure that the hex files generated by different versions of the compiler remain unchanged? As follows:

--

Thanks & Regards

Yale

  • How can we ensure that the hex files generated by different versions of the compiler remain unchanged?

    What you ask is not possible.

    When the compiler changes it is usually because the vendor (TI) has improved its efficiency. I.e. for the same source code, a smaller number of assembly instructions are generated to implement the behaviour described by the source code. Sometimes a corner case bug might be fixed which also changes the assembly code.

    It is up to the end user through Configuration Management to make sure the same compiler is always used and/or to carefully assess a new compiler's changes.

  • The good news is that you can stop someone from using the wrong compiler with the following code:

    #if __TI_COMPILER_VERSION__ != 22000000
        #error You have the wrong compiler configured!
    #endif

  • How can we ensure that the hex files generated by different versions of the compiler remain unchanged?

    Kier is correct.  This is not possible.  To be honest, I'm surprised the map file matches as much as it does.  Typically, many changes are seen.

    Thanks and regards,

    -George