This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TIEVM-HV-1PH-DCAC: Circuit design issues

Part Number: TIEVM-HV-1PH-DCAC

My customer has the following needs and wants you to help him with his design.

Condition:

1.Input voltage DC 12V or 24V .

2.The output voltage is expected to be an AC 60V and -60V .

3.Frequency 50Hz or 60Hz is acceptable .

That's what the customer needs .

Thanks.

Boyan