Part Number: INSTASPINFOCMOTORWAREGUI
Hi Team,
I would like to ask for some clarifications on the document SPRUHJ1I. Section 5.1 software prerequisite mentions that to select a proper IQ full-scale voltage the document says that it should be 20 to 30% more than the maximum value but it also says that the maximum value should be calculated based on motor flux. So which should be considered as the maximum value based on motor flux is 20 and the maximum voltage in the motor with back emf is 48V.
Can you please help clarify?
Thank you
Regards,
Marvin