This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TI programmer's boot loader upload switching between MCU 1 and MCU 2

Provide case details or comments:

  1. We need to get the checksum to compare it to the correct value.
  • I can read the checksum code, but I can't extract the value

Can you please help us?

Programmer : XDS110

MCU 1 : F280040PMQR

MCU 2 : F280048PMQR

@echo off
setlocal
setlocal ENABLEDELAYEDEXPANSION

REM Path to this batch script
set UNIFLASH_PATH=%~dp0

REM Path to DebugServer folder
set DEBUGSERVER_ROOT=%~dp0ccs_base\DebugServer\

set MODE=flash
set EXECUTABLE="!DEBUGSERVER_ROOT!bin\DSLite"

set GENERATED_COMMAND=-c user_files/configs/f280040.ccxml -l user_files/settings/generated.ufsettings -s VerifyAfterProgramLoad="No verification" -e -f -v -a CalculateChecksum "user_files/images/Bmw_DcDcLlcx40_FBL.hex" 
set ADDITIONALS=


REM list available modes
if "%1"=="--listMode" (
	echo.
	
	echo Usage: dslite --mode ^<mode^> arg
	echo.
	
	echo Available Modes for UniFlash CLI:
	echo   * flash [default] - on-chip flash programming
	echo   * memory          - export memory to a file
	echo   * load            - simple loader [use default options]
	echo   * serial          - serial flash programming
if exist !DEBUGSERVER_ROOT!drivers\MSP430Flasher.exe (
	echo   * mspflasher      - support MSPFlasher command line parameters [deprecated]
)
	
	exit /b 0
)
 
CMD /S /C "%EXECUTABLE% !MODE! !ADDITIONALS!"

REM no parameters given, use the default generated command
if "%1" EQU "" (
	echo Executing default command:
	echo ^> dslite --mode !MODE! !GENERATED_COMMAND! !ADDITIONALS!
	echo.
	 
	CMD /S /C "%EXECUTABLE% !MODE! !GENERATED_COMMAND! !ADDITIONALS!"
	exit /b !errorlevel!
)

REM user options parsing
set USEROPTIONS=%*

REM user options without the --mode
set "_args=%*"
set "_args=!_args:*%1 =!"
set "_args=!_args:*%2 =!"

if "%3"=="" (
	set USEROPTIONS2=
) else (
	set USEROPTIONS2=!_args!
)

REM custom mode from users
if "%1" EQU "--mode" (
	set MODE=%2
	set USEROPTIONS=!USEROPTIONS2!
)

REM default user options if none given
if "!USEROPTIONS!" EQU "" (
	set USEROPTIONS=-h
)

REM mspflasher support
if "%MODE%" EQU "mspflasher" (
	set EXECUTABLE=!DEBUGSERVER_ROOT!drivers\MSP430Flasher.exe
	set MODE=
)

REM execute with given user parameters
echo Executing the following command:
if "!MODE!" EQU "" (
	echo ^> !EXECUTABLE! !USEROPTIONS! !ADDITIONALS!
) else (
	echo ^> !EXECUTABLE! !MODE! !USEROPTIONS! !ADDITIONALS!
)
echo.
echo For more details and examples, please visit https://software-dl.ti.com/ccs/esd/uniflash/docs/latest_qsguide.html#command-line-interface
echo.

CMD /S /C "%EXECUTABLE% !MODE! !USEROPTIONS! !ADDITIONALS!"

exit /b !errorlevel!