Hello,
i think this topic exists a hundred times but I couldn`t solve the problem anyway.
On a F28335 i implemented a 3 ph PMSM FOC for my Bachelor Thesis. My problem is the eCAN Baudrate. Everything works fine with the preconfigured 1Mbit/s setting which is
Baudrate Prescaler: 5
TSEG1: 8
TSEG2: 6
I want to set the CAN bus to 500kbit/s but if i change the Baurate prescaler in the Simulink configuration block "F28335 eZdsp" I get the message "Assertion failed".
Could someone verify my settings which are:
BRP = 10
TSEG1 = 10
TSEG2 = 2
Did someone encounter the same problems programming the DSP with the Target Support Package?
Regards,
Maxi