Other Parts Discussed in Thread: TMS320F28234, CONTROLSUITE
I have a problem with the XINTF interface of the TMS320F28234 and Code Coposer Studio 4.1.2
I connect the target board and load the software to the target (SARAM). With the debugger I "Go to main" and the main is reached in the debugging code.
If then I select the "scipt XINTF_enable" I can read and write to the external memory in the memory register. I also can fill the external memory with different data values and also can read it back.
If I configure in software the same registers with the same values as it is done by the script and I stop the code immediately after this initialisation (breakpoint) it is not possible to read or write to external memory. I´ve also checked this registers that their values are like they are configured by code.
Can you please give me an idea what can be the reason for?
Best regards
Mathias