Part Number: TMS320F28386S
Other Parts Discussed in Thread: C2000WARE
Hello,
Using simple UDP communication built on the example code from C2000Ware V 4.01.00.
I get after about 20 minutes of work
the code breaks at line 323 of f2838xif.c
pktDescOrigPtr = mem_malloc(sizeof(Ethernet_Pkt_Desc));
mem_alloc_count++;
if(pktDescOrigPtr == NULL)
{
pbuf_free(p);
LINK_STATS_INC(link.memerr);
__asm(" bkpt #0");
return (ERR_MEM);
}
I have seen that there are some discontinues on memory leak. but on different places on this file.
I compared this file to the file on the latest C2000ware version 4.03.00.
the files are the same. seams like no fix was updated.
Please help.
I have devices getting stuck on customers site.
Thanks!