Part Number: TMS320F28375D
Hi team,
I am using HRPWM with TMS320F28375D.
PWM is generated by setting CMPA/CMPB using up/down counters.
We have manufactured many identical boards, but only one of them has the following phenomenon.
What are the possible causes?
(Occurs once a day. Does not occur if HRPWM is not used)
・PWM of about 20ns is output even though CMPA/CMPB is not controlled.
・Even though the TRIP signal is input and the gate driver is turned off, PWM of about 20ns is output.

CH1:ePWM5(Hi SIDE)
CH2:ePWM5(Lo SIDE)
CH3:ePWM6(Hi SIDE)
CH4:ePWM6(Lo SIDE)
CH5:ePWM8(Hi SIDE)
CH6:ePWM8(Lo SIDE)
CH7:NOT USE
CH8:TRIP SIGNAL
Best regards,
Takahashi