This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F2800157-Q1: Behavior of action qualifier T1

Part Number: TMS320F2800157-Q1

Hello, 

In one of application I am using digital compare sub module and one of the DCxEVTY is linked to the action qualifier T1.
Now Latch of DCXEVTY is enabled(cleared at period). Assume, I am making PWM high at counter = 300, and making PWM low at T1U event. (counter running from 0 to 499)
Now, if DCXEVTY is occurs at counter = 200, and as latch is enabled it persist till counter = 499.

My doubts are:

1) is T1U only occurs at counter = 200(Only at one instance) or it keeps active till 499 count and once PWM becomes high at counter =300 it reset to 0 immediately?

2) If T1U only active only at counter = 200, then I should see high pulse for 300 to 499 count and if it persist continuously then ideally I should get continuous low pulse (which type of PWM it will provide as output?)

Thank you. Regards,