Part Number: TMS320F28378S
Hi,
We are designing for TMS320F28378SPZP (100-pin QFP).
We see in the datasheet "During the ramp, VDD should be kept no more than 0.3 V above VDDIO". VDDIO is typically 3.3V, VDD is typically 1.2V. Is it therefore acceptable to power up all 3.3V supplies and then all 1.2V supplies?
We are using two separate DC / DC converters to originate 3.3V and 1.2V. In our current design, the 3.3V converter PGOOD signal drives the enable line on the 1.2V converter; 1.2V does not power on until 3.3V powers on. Is this acceptable?
Thanks!