This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28022-Q1: What are root causes for pre-condition failed?

Part Number: TMS320F28022-Q1

Hi BU, 

Customer side met 2 chips can't be erased (returned from customer's field, i.e. car OEM). They tried to use On-Chip Flash tool to erase the chips, and 1 chip returns erasing error -21, that is pre-condition failure. 

Since pre-condition is after pre-compaction, so that means this chip is not in over-erased or "depletion" state. Am I right? 

And I let them give me the Flash contents for this chip, you can check from: https://e2e.ti.com/cfs-file/__key/communityserver-discussions-components-files/171/C1_5F00_sections_5F00_not_5F00_erasable.bin

As you can see from the above bin file, the section B for this chip is almost 0's, that is the clear stage for erasing process. However, there is some bits can't be cleared as following fig shows: 

I want to check with you what are the possible root causes for this pre-condition error? Could it be Flash memory cell HW failure? If it is, we need to do failure analysis and at the mean time need to check the application root cause for this failure. Please give your guidance, thanks. 

Regards, 

Will