Part Number: LAUNCHXL-F28379D
Other Parts Discussed in Thread: TMDSCNCD28379D
Hi Team,
I have a question from a customer regarding the use of F28379D. Please see below:
We are using F28379D control stick for our high-power inverter (100kVA) application.
To interface this control stick with our 100kVA inverter, we have designed a board in that PWM level shifter, op-amp circuits for voltage and current sensing etc., will be there.
Some MOSFET'S got failed due to some reasons, at the same time F28739D control stick also got failed all the time.
We can't understand why the control stick got failed.
My questions are:
1. is this F28379D control stick suitable for high power applications or only design and verification purpose?
2. If it is suitable, we want to know what are the possibilities of failing of control stick or else do we need take any precautions or do we need to add any protection circuits?
3. If it is not suitable, how can we proceed with F28379D for our high power applications?
Please let me know if you need more information.
Regards,
Marvin