This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28335: TMS320F28335

Part Number: TMS320F28335
Other Parts Discussed in Thread: TLV757P,

Dear Experts,

We have a controller board based on the F28335 DSP. We are using 1.8V for core voltage. Now we want change it to 1.9V. Selected the part no TLV75719PDBVR. The selected part no has 1.9V, 1A output rating. We are seeing fixed output voltage regulator. Is the selected part no serve the purpose or any other alternates available. We are searching for fixed voltage regulators rather than adjustable regulators.

With Regards,

Balaramkumar