Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE, TMDSCNCD28335
Dears,
The customer uses a separate power supply when using 28335
If the 3.3V transistor in the level shift buffer of the I/O PIN is powered on before the 1.9V transistor, it may cause the output buffer to open, causing a false pulse at the moment of power-on.PLs help to check it?
Pls kindly find attach file for the wave form.
CH1:IGBT Driver Wave form
CH2:1.9V Wave form
CH3:PWM Wave form
CH4:3.3V Wave form
Highlight red is the false pulse wave form
Thanks