Other Parts Discussed in Thread: C2000WARE
Hello,
I was trying to program on Simulink but i will get this error:
(Error -2131 @ 0x0) Unable to access device register. Reset the device, and retry the operation. If error persists, confirm configuration, power-cycle the board, and/or try more reliable JTAG settings (e.g. lower TCLK)
Here is the hardware setting I have.

I have tried with "Use internal oscillator" was not working. I have tried to unclick the "use internal oscillator" and lowered the "oscillator clock (OSCCLK) frequency in Mhz"and still does not work.

I double-checked with my external mode port is connected to the correct one, the sample and duration is matched as 8, and the bits per second is also matched.


The boot mode (S3) is default 11, which is boot from flash. SEL1 (S2) is default 00, and QEP (S5) is default 11. The CAN Route (S4) is low (i tried high as well).
I have tried unplugging and plugging back to reset the board, as well as using the reset button. I also created new simulink file and still not working.
I also tried to power the board using an external power supply and an external XDS110 JTAG debug probe, not using the usb. It was still not working.
I have used the F280025C launchpad before and it worked successfully, so I tried all the possible things that I have tried on that launchpad with this launchpad, but it's still not working.
Rinya