Part Number: TMS320F28034
Other Parts Discussed in Thread: C2000WARE
Hi Champ,
I am reconfirming the missing external crystal behavior on F28034 for my customer.
Since my customer is facing the clocking source - external crystal oscillator be interfered by high frequency, then DSP is died. In this condition, the JTAG cannot be connected, and it can only be fixed after re-power on.
(1). Referred to below thread, may I reconfirm the answer would be the same on F28034, correct ?
On missing clock condition, PLL is forcefully bypassed and OSCCLK source is switched to INTOSC1 (10MHz). After missing clock, we do need to reconfigure PLL in NMI interrupt, then
continue running the application code.
(2). Besides, do we have any examples for that on F28034 ? I didn't see there is the one for F28034 in example.
(3). Is there any cautious on the hw design besides referring to Figure 8-8. Using the On-chip Crystal Oscillator ?
Thanks and regards,
Johnny