Part Number: LAUNCHXL-F280039C
Other Parts Discussed in Thread: UNIFLASH
Hello,
I am currently working on a launchpad to upload a program to flash and leave it running. I could not be able to run the program in flash until I found out that the booting switch was wiggling. After fixing that, I could use the launchpad with standalone operation. However, while I was investigating about the problem, I tried the uniflash tool. It said to update de debugging probe to a newer version. The problem now comes when I use CCs version 12.2 that I am no longer able to debug the launchpad.
I have searched for different solutions and I am still not able to program the launchpad. I will give some context about mi current situation:
First, the drivers do not appear in device manager so they can not be uninstalled and I could not find a webpage to download them. Furthermore, I tested connection with the XDS110 in another PC and did not work wither.
Second, I tried the xdsdfu to revert the firmware version and could not connect to any target.
I would like to know which is the best solution to that problem. Also, I woudl like to know if it is possible to reset the debugger without the need of hardware modifications.
Regards,
David