This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
The data sent to the left and right channels through DRR1 and DRR2 (16 bits each) are output by the DAC of the audio chip into sine waves. In the case of different values, the two headset sound channels have the same value, and it seems that the value of DRR1 is used, and the value of DRR2 is directly invalid.
AIC23 set the main mode and left and right channel update has been opened, it seems to be the Master mode USB mode BCLK=MCLK DSP mode 16-bit input data length, I do not know much about this overall process, if there is a document, I hope to recommend it, thank you!!
Reference document: 320AIC23.pdf
Would like to ask seniors to help guide or provide some reference routines, thank you!
AIC23 and DSP are configured as follows:
AIC23 register Settings:
AIC23Write(0x00,0x00);
Delay(100);
AIC23Write(0x02,0x00);
Delay(100);
AIC23Write(0x04,0xff);//Earphone left channel control
Delay(100);
AIC23Write(0x06,0xff);//Earphone right channel control
Delay(100);
AIC23Write(0x08,0x14);//Analog audio path control
Delay(100);
AIC23Write(0x0A,0x00);//Digital audio path control
Delay(100);
AIC23Write(0x0C,0x00);//Power off control
Delay(100);
AIC23Write(0x0E,0x43);//Digital audio interface format looks like Master mode USB mode BCLK=MCLK DSP mode 16 bit input data length.
Delay(100);
AIC23Write(0x10,0x1f);//Sample Rate Control clock is USB mode
Delay(100);
AIC23Write(0x12,0x01);// Digital Interface Activation
Delay(100); //AIC23Init
McbspaRegs.SPCR1.all=0;
McbspaRegs.SPCR2.all=0;
McbspaRegs.SPCR1.all = SPCR10_VAL;
McbspaRegs.SPCR2.all = SPCR20_VAL; //When the simulation stops, the serial clock continues to run
McbspaRegs.PCR.all = PCR0_VAL; //Rising edge sampling
McbspaRegs.XCR1.all = XCR10_VAL;
McbspaRegs.XCR2.all = XCR20_VAL;
McbspaRegs.RCR1.all = RCR10_VAL;
McbspaRegs.RCR2.all = RCR20_VAL;
McbspaRegs.DXR1.all = 0;//clear data
McbspaRegs.MFFINT.bit.RINT = 1;//Interrupt management
McbspaRegs.SPCR1.bit.RRST = 1;//Open serial port reception
McbspaRegs.SPCR2.bit.XRST = 1;//Enable serial port transmission
Hi,
I will assign this thread to the expert who will provide the response at the earliest.
Regards,
Meghavi
Hello,
I've reassigned this to the proper expert, but due to the July 4th holiday they will be out-of-office until at least Wednesday. Please expect a reply after that.
Best regards,
Omer Amir
Just to confirm, the target DSP SW is being run on the F2833x C2000 device vs the original C54x DSP? Is the question that the code is not behaving as expected on the C2000 or that in general code support for the AIC23 driver and its operation? This kit is not owned by C2000 team, and we might need to get it re-assigned based on your reply.
Best,
Matthew