Part Number: TMS320F280039C
Other Parts Discussed in Thread: C2000WARE
While reviewing the flash and boot rom specifics for the F280039C I've run into inconsistent information and would like to understand what the differences mean.
This is regarding the base address for the Boot ROM.
Two documents cited are:
TMS320F28003x Real-Time Microcontrollers datasheet (Rev. B)
TMS320F28003x Real-Time Microcontrollers Technical Reference Manual (Rev. B)
The details of the start address are different one states 0x3F0000 the other 0x3F8000, is one a typo? If so, which one? Or are both correct, and how are these differences to be used?
from sprsp61b:
from: spruiw9b: