This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28388D: The program stuck in _IQ16sqrt and _IQ16sin

Part Number: TMS320F28388D

Hi Team,

My customer use IQMATH in his project. He add these two functions to ePWM ISR.

The program work normally during debug. And stuck in these two functions after he loaded the program to FLASH. Because the toggle LED operation in main function is not operated. 

Then he delete these two functions and program works normally.

--

Thanks & Regards

Yale

  • Yale,

    I have seen this exact issue occur with another customer in the past. In their case, the IQMath library as well as the IQMathTables were resident in RAM, which were lost on Power cycle. Can you check if the same thing is occurring here?

    Why are they setting MATH_TYPE = IQ_MATH and not FLOAT_MATH even with a floating point device?

    Thanks,

    Sira