Sir:
I want to use MATLAB / Simulink 2010a to deploy my real time application on DSP f28035 EVM. But when i build the simulink model, i always get the following error message:
The call to idelink_ert_make_rtw_hook, during the exit hook generated the following error:
Error while loading and running the project.
The build process will terminate as a result.
and,
when i typed at the MATLAB prompt "checkEnvSetup('ccs','f28035')", i got the following incompitability errors of CCS v3.3 as depicted below:
>> checkEnvSetup('ccs','f28035')
1. Checking CCS (Code Composer Studio) version
Required version: 3.3.82.13
Required by : Embedded IDE Link 4.1
Required for : Automation and Code Generation
Your Version : 3.3.83.19
Incompatible version detected. CCS version does not satisfy product requirements!
2. Checking CGT (Texas Instruments C2000 Code Generation Tools) version
Required version: 5.2.1
Required by : Embedded IDE Link 4.1
Required for : Code generation
Warning: Illegal right hand side in assignment. Too many elements.
> In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>envSetup at 285
In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 68
In checkEnvSetup at 131
Your Version :
Incompatible version detected. CGT version does not satisfy product requirements!
3. Checking DSP/BIOS (Real Time Operating System) version
Required version: 5.33.05
Required by : Embedded IDE Link 4.1
Required for : Real-Time Data Exchange (RTDX)
Warning: Illegal right hand side in assignment. Too many elements.
> In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>envSetup at 285
In C:\Program Files\MATLAB\R2010a\toolbox\idelink\extensions\ticcs\envChecker\checkEnvSetup_private.p>checkEnvSetup_private at 68
In checkEnvSetup at 131
Your Version :
Incompatible version detected. DSP/BIOS version does not satisfy product requirements!
How can i solve this incompitability problem? I installed the attatched version of CCS v 3.3 with the DSP EVM. What is the problem now?
Note that i am using windows vista.
Please tell me what to do to solve this problem ASAP.
Thanks,
Eng. Dina