Part Number: F28M35H52C
Hi,
We would like to use the FLASH API,
currently we are following TI examples and copying the FLASH API to RAM,
we can see it takes ~6K of RAM,
would it be possible to somehow reduce this size of used?
1. maybe it is possible to run FLASH API without copying it to RAM?
2. maybe it is possible to cherry pick specific FLASH API functions to reduce RAM memory used?
Thanks,