Part Number: TIDM-1000
Hello, Experts,
This is for my customer; the front-end converter is 3 phase PFC with 3 PFC chokes and 6 Mosfet operated using SVPWM without neutral. But customer asking for neutral line, they argued that neutral can bypass unbalanced current in case of any disturbance happened.
Qn1: Incase if there is no neutral if an unblance happen; what will be the after effect ?
Qn2: if the grid is unbalanced (say RY phase 420Vac, YB phase 400Vac) and there is no neutral. weather my controller will taken care ? (by making proper adjustments in the modulating signal ) ?
Qn3: If i am taking neutral? how it is being connected to the converter without changing the topology. ? Spitted DC link capacitor with neutral at the middle point. ?
Thanks and regards
Anoop kumar