Other Parts Discussed in Thread: UNIFLASH
After using the DCSM module to encrypt the flash of 280025, the jtag cannot be connected again, and uniflash is also useless
I have configured the zone per linkpoint section in the DCSM module ZONE1, and set a password (not all zeros) to transfer all sectors of flash to zone 1 protection, without configuring ZONE2. After the configuration is completed, build the project, connect the development board, burn the program, and then use the MEMERY browser to view the memory. At this time, the console will output security: true
Later, I used tool-on chip flash to unlock, and the console displayed security: false. I clicked program xx again (the option next to unlock, lock) to exit the debug state and connect again. An error was reported indicating that the device is in low power state. Do you want to forcibly wake it up
I encrypted through configuring the DCSM GUI interface without writing a program
The following is an error prompt