This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280049C: SPI FLASH and program

Part Number: TMS320F280049C

Hi TI support team 

1. If booting through the SPI interface's Flash, do you have any special requirements for the flash connected to the SPI?

2. Can the boot program still be started through SPI when multiple memories are connected using the slice selection function?

3. How to convert. hex to a. bin file that can be program to F280049?

3. How to send .bin files and program them into the F280049