This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F28379D: GUI disconnected while giving clear trip in build 1 (3-Phase Vienna Rectifier)

Part Number: TMS320F28379D
Other Parts Discussed in Thread: SFRA, POWERSUITE

Using TMS320F28379D, 3-phase vienna rectifier while giving clear trip in build 1 (open loop) using JTAG communication from CCS GUI, the GUI gets disconnected and XRS pin of the TMS320F28379D was pulled low. I has probed the +3.3V-VDD and +3.3V-VDDOSC both were observed with PWM frequency noise (frequency at which PWM generating from the DSP).

GUI shows pop up as CPU is in hibernate or low power mode. Do you want to wake-up the micro controller. It seems like this error was due the XRS pin pulled low after giving clear trip.

Can you help with this what may be the reason for the above behaviour.