Part Number: TMS320F28379D
Greetings,
I have two projects, both of which are using the XDS100 v3 debug probe. I can connect to the target with one but not the other. The one which connects is setup to connect while the system is running. The one which does not is setup to overwrite the flash. In both cases, the HW is identical, and both projects are in the same instance of CCS. When it fails, I get the following dialog box. What could be causing the failure.

Thank you,
Ed