Other Parts Discussed in Thread: CONTROLSUITE
Hi Everybody,
I would like to realize a project with a buck boost power supply. Therefore I would like to use the TI DP library within ControlSuite.
- I am using the DPLibTemplate-F2803x as the starting point for my development.
- After importing this project into CCSv4 the build process was successful.
- In the next step I tried to add the PWMDRV_BuckBoost module as it is described in the DPLib.pdf. I included the correct new search paths for the include and asm folders, because of the new version f2803x_v3.2, where the PWMDRV_BuckBoost module is in. The original template is using f2803x_v3.0.
- I changed the search paths before modifying the template to make use of the PWMDRV_BuckBoost module to make sure that the original template works with the new version f2803x_v3.2. This build was successful too.
- If I now insert the necessary code into the template to use the PWMDRV_BuckBoost module I get the following erros, which reside in the ProjectName_DPL-ISR.asm or PWMDRV_BuckBoost.asm respectively.
Console Output:
"../ProjectName-DPL-ISR.asm", ERROR! at line 78: [E0009] Missing struct/union member or tag MOVW DP,#_EPwm:m:Regs.CMPA "../ProjectName-DPL-ISR.asm", REMARK at line 78: [R0001] After symbol substitution the line became: MOVW DP,#_EPwmRegs.CMPA "../ProjectName-DPL-ISR.asm", ERROR! at line 78: [E0009] Missing struct/union member or tag MOV @_EPwm:m:Regs.CMPA.half.CMPA,AL "../ProjectName-DPL-ISR.asm", REMARK at line 78: [R0001] After symbol substitution the line became: MOV @_EPwmRegs.CMPA.half.CMPA,AL "../ProjectName-DPL-ISR.asm", ERROR! at line 78: [E0003] Syntax error - Operand 2 MOV @_EPwm:m:Regs.CMPA.half.CMPA,AL "../ProjectName-DPL-ISR.asm", REMARK at line 78: [R0001] After symbol substitution the line became: MOV @_EPwmRegs.CMPA.half.CMPA,AL "../ProjectName-DPL-ISR.asm", ERROR! at line 78: [E0004] Not expecting AX operand MOV @_EPwm:m:Regs.CMPA.half.CMPA,AL "../ProjectName-DPL-ISR.asm", REMARK at line 78: [R0001] After symbol substitution the line became: MOV @_EPwmRegs.CMPA.half.CMPA,AL "../ProjectName-DPL-ISR.asm", ERROR! at EOF: [E0300] The following symbols are undefined: CMPA _EPwmRegs Errors in Source - Assembler Aborted I would very appreciate any kind of tips in order to get rid of these errors. I am not very familiar with programming in assembly, so I can not really think of the reasons for these errors. Thank you and best regards, Gregor