Part Number: TMS320F280038C-Q1
Hello,
We are migrating from a f280049 DSP to a f280038 and I noticed in the reference manual there isn't a disclaimer saying there's a 2 cycle delay between SYNC Pulse and slaves updating their TBCTR values like there was in the 280049. Can you confirm the 28003 do not have this inherent 2 cycle delay that requires TBPHS = TBPHS_DESIRED+2. Also the f280049 (as well other models we've worked with like the f28379) had synchronization chains (see second picture) where only certain PWMs could sync downstream ( e.g PWM4 could sync off of PWM1, but not vice versa). Is this limitation also gone on the 28003 in that PWM4 could sync off of PWM1, but also, with a different setup, PWM1 could sync off of PWM4?