Part Number: TMS320F28P650DK
Other Parts Discussed in Thread: C2000WARE
hi,
The follwoing sci example C:\ti\c2000\C2000Ware_5_00_00_00\device_support\f28p65x\examples\cpu1\sci\sci_ex1_echoback.c is not working for F28p65x.
I went through the documentation aand ensure S1 both positions are set to on'.
Please let me know if I have to take care of any other settings.
Also, the position of S1 in the actual board is differnt from the documentation. Int hedocumentation , it says S1 is on the back side, however, in the actual board, it is on the front side.
Thanks,
Mukul