This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TMS320F280039C: STL_CLA failing at POST Test Vector 08

Part Number: TMS320F280039C

Dear expert,

I am trying to run the SW Test of CLA in my evaluation board and it is currently failing. I noticed the onliny failing test is the SPI test which I believe is Test Vector 8 and the  returned status is 0x23, which means CLA STL overflow  and PSA1 and 2 failing. 

Can you foresee any reason why only this test would fail? Is there any special conrfiguration required for this test?

Furthermore, we are building our code in COFFABI format, therefore I modified the library files to adapt to COFFABI. I already did this on the past, so I am not expecting this to be the root cause of the issue.

Thanks in advance,

Marc Ferrer