Part Number: TMS320F28069
Hello,
I would like to use ADCINAx or ADCINBx pins like GPIO pins.
How can I use?
How can I init these pins like a GPIO pin?
For Ex;
I want to define ADCINA7 pin as GPIO, input/output etc...
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: TMS320F28069
Hello,
I would like to use ADCINAx or ADCINBx pins like GPIO pins.
How can I use?
How can I init these pins like a GPIO pin?
For Ex;
I want to define ADCINA7 pin as GPIO, input/output etc...
Hi Mert, unfortunately ADCINA3, A5, and A7 cannot be configured as GPIO. To determine which analog inputs can be configured, please review the "Signal Descriptions" table in the device datasheet: https://ti.com/lit/SPRS698.
For other analog inputs which can be configured, please look into the AIOMUX1 register which is documented in the technical reference manual: https://ti.com/lit/SPRUH18
Regards, Joe