Other Parts Discussed in Thread: SYSCONFIG
is some of C2000 series micro controllers pin compatible with each other
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: SYSCONFIG
is some of C2000 series micro controllers pin compatible with each other
Hello Leela,
There are some devices which have certain pins compatible with each other, but this depends on the device (you can view the migration guides that are included on the product page in the Technical Documentation section). I do not believe there is a device with a 100% pin compatibility, but depending on what pins you are using you can likely find how to migrate from one device to another. If you are planning on migrating, I recommend using SysConfig if possible since this will simplify what peripherals can be used and what pins are not available on the device which is being migrated to.
Best regards,
Omer Amir