Part Number: TMS320F28335
Other Parts Discussed in Thread: TMDSDOCK28335, CONTROLSUITE, TMDSCNCD28335
Hi all,
I am using TMDSHVMTRPFCKIT with F28335 for PMSM motor control.
Errors show while external AC power is ON, the errors in Console are as follows:
C28xx: Error: (Error -1041 @ 0xFFFFFF66) The debug probe reported an error. Confirm debug probe configuration and connections, reset the debug probe, and retry the operation. (Emulation package 9.9.0.00040)
C28xx: Trouble Halting Target CPU: (Error -150 @ 0x0) One of the FTDI driver functions used during configuration returned a invalid status or an error. (Emulation package 9.9.0.00040)
C28xx: Unable to determine target status after 20 attempts
C28xx: Failed to remove the debug state from the target before disconnecting. There may still be breakpoint op-codes embedded in program memory. It is recommended that you reset the emulator before you connect and reload your program before you continue debugging
And the probe seems to be disconnected as the errors showed. The expression show as the figure below:

Also, when I try to run the code without the AC power or using a TMDSDOCK28335, it works just fine.
What could be the cause and how do I resolve this?
Btw, I can't add TMDSHVMTRPFCKIT as Part number for the thread.