Part Number: TMS320F28335
Other Parts Discussed in Thread: C2000WARE
The previous response did not help.
I got this error when building the project in CCS version 12.3.0.00005.
"This project was created using a version of DSP/BIOS tools that is not currently installed: 5.41.10.36. Please install the DSP/BIOS tools of this version, or migrate the project to one of the supported versions."
The project was originally built on CCS version 4.2.3.00004
Now, what is the best and least risky path forward ? To install & upgrade the BIOS to a newer version and build or migrate the project within the ccs 12.x ? For both scenarios, I need the site to download any files (as applicable) and procedure to upgrade or migrate. I could not find anything in the CCS menu to do so. The "Project > Properties > DSP/BIOS version:" I only see drop-down selection for 5.41.10.36
Thanks